AXIS#.IL.IFOLD

Description

Two current foldback algorithms run in parallel in the drive: the drive foldback algorithm and the motor foldback algorithm. Each algorithm uses different sets of parameters.

Each algorithm has its own foldback current limit, AXIS#.IL.DIFOLD and AXIS#.IL.MIFOLD. The overall foldback current limit at any moment is:

AXIS#.IL.IFOLD = min (AXIS#.IL.DIFOLD, AXIS#.IL.MIFOLD, AXIS#.IPEAK)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

A

Range

0 to 2,147,483.647 A

Default Value

N/A

Data Type

Float
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
AXIS1.IL.IFOLD

500ah

0ch

Signed32

-

1000:1

Read only

No

AXIS2.IL.IFOLD

510ah

0ch

Signed32

-

1000:1

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.IFOLD

5809

16B1

Signed32

Read Only

-

AXIS2.IL.IFOLD

71345

116B

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.IFOLD

5809

Float

Read Only

-